4/1/2014 4:32 PM | |
Joined: 7/29/2008 Last visit: 10/12/2024 Posts: 96 Rating: (4) |
I am using for the first time SCALANCE S612 (V4) and Softnet Security Client (V4+HF1). I would like to access a SIMATIC PLC/HMI network (NETWORK ID 192.168.3.0) remotely through VPN with a static IP using a router with portforwarding to s612 (UDP 500, UDP 4500). After following tutorials with no success. http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=22056713&objAction=csOpen&lang=en&siteid=cseus&aktprim=4&extranet=standard&viewreg=WW http://support.automation.siemens.com/WW/llisapi.dll?query=22056713_S612_VPN_DOKU_V30_en&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=&nodeid4=20229805 SCALANCE S612 cannot be reached remotely through internet even through the security configuration tool online mode. WAN IP static address router IP 10.30.130.1 SCALANCE external IP 10.30.130.40 SCALANCE internal IP 192.168.3.210 Attached are pictures from the security configuration tool (V4). As for VPN tab, Wait for partner (responder) is selected and the WAN IP address is the public static WAN address. Any help will be greately appreciated.
Attachmentscalance_config.pdf (458 Downloads) |
4/3/2014 4:35 PM | |
Joined: 7/29/2008 Last visit: 10/12/2024 Posts: 96 Rating: (4) |
I did use wireshark but did not capture any ISAKMP packets. What does this mean?
|
Follow us on