4/24/2014 4:02 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170)
|
Please add the SIA logfile from %autinstlog% (just enter in START > RUN) here. |
Have Fun! |
|
4/24/2014 6:18 PM | |
Joined: 11/21/2013 Last visit: 12/11/2023 Posts: 5 Rating: (0) |
Is this the file that you are looking for? The txt file couldnt be uploaded so I zipped it. Thanks again, Ruben.
AttachmentSIA_Starter.zip (695 Downloads) |
4/25/2014 2:59 PM | |
Joined: 11/21/2013 Last visit: 12/11/2023 Posts: 5 Rating: (0) |
There are many SIA logs within that folder. Please find the latest SIA Step 7 Pro V13 as an attachment.AttachmentSIA_STEP7_PRO_V13@14-04-24_12-12-16.zip (644 Downloads) |
4/25/2014 7:54 PM | |
Joined: 11/21/2013 Last visit: 12/11/2023 Posts: 5 Rating: (0) |
Hi, I went through theSIA*.log from the Setup folderand located the section where the error was found. As you can see below, it appears that a program installed in my computer was conflincting with the installation process... I deleted this program (I no longer need it), restartred my computer and the installation wassuccessfullycarried out. Many thanks toTomDeWoufor this help in locating the log file. - Ruben. ______________________________________________________________________ ######## ---------- START SECTION ------------------------- #################### ######## ENVIRONMENT ANALYSE #################### ######## -------------------------------------------------- #################### 11:41:06|INFO1 |BusinessLogic::Install() |(01) Environment analyse finished with Message: Success 11:41:06| |MsiEnvironment::Initialize() | 11:41:06| |MsiEnvironment::Initialize() |(07) START analyse of the MSI environment 11:41:06|.... |MsiEnvironment::AddProductByCode() |(07) Analyzing: ProductcCode: {6EB41708-7B48-46A7-8552-53BDD25EF3DC}; Local package: C:\Windows\Installer\64cffa6.msi; Name: ALFA PROGETTI s.r.l. 11:41:06|... |MsiEnvironment::AddProductByPath() |(07) Exception - SetupException Siemens.Automation.Setup.Core.SetupException: Release Version string is empty. |
This contribution was helpful to1 thankful Users |
8/1/2014 6:14 AM | |
Posts: 1 Rating: (0) |
Which program you deleted? V12? |
8/31/2014 7:39 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
new question published by WeeHongis split to a seperate thread with the subjectwhere do I find this SIA logfile and %autinstlog%?. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
9/12/2014 11:23 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on