6/28/2016 12:05 PM | |
Posts: 2 Rating: (0) |
Hi Murof, Thanks for noticing my query. yes I have same wincc v7.2 which aspire89 had. and when i try to browse server it gives the same error "The OPC Server Does not supports a browser interface" OPC Server I use is B&R PLC X20CP3585 which supports OPC UA Server in it and Software Name is Automation Studio 4.2.3. Now the point is this B&R PLC is communicating with Our siemens OPC Scout v10 and OPC Scout is reading the tags of B&R PLC through OPC UA Configuration but WinCC is Just Creating a Certificate and not Communicating. Below is the Snapshot of OPC Scout and third party B&R PLC OPC UA Configuration. If You have any Solution or some proper Procedure for this Please Give me a Solution. AttachmentBnR And OPC Scout Config.zip (324 Downloads) |
4/4/2017 3:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by frederico.inese is split to a separate thread with the subject Get tag in OPC UA Server from TP1200. Best regards |
9/18/2017 4:15 PM | |
Posts: 25 Rating: (3) |
WinCC 7.4 OPC UA SERVER instruction https://www.youtube.com/watch?v=uiOhnr5Lpxw OPC UA is very useful for me, no need to config DCOM, share for you PHAM XUAN KY |
9/19/2017 8:21 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641) |
Hello I think you should use the official Link, and there is also a Siemens video: https://support.industry.siemens.com/cs/ww/en/view/109479664 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on