Industry Online Support
Technical Forum
4/27/2014 5:49 PM | |
Posts: 133 Rating: (0) |
hello, How can I write 0 or 1 in BIPOLAR pin of FC105 ? thanks |
4/27/2014 6:20 PM | |
Posts: 167 Rating: (4) |
Hi you can assign a memory bit to bipolar pin and assign 1 or 0 to memory bit. best regards, Poya_xp
|
4/27/2014 6:22 PM | |
Posts: 133 Rating: (0) |
That is the point, how assign a constant value to a memory bit ? |
4/27/2014 6:23 PM | |
Posts: 133 Rating: (0) |
what!, you tell me that M0.0 is by default '0' ? |
4/28/2014 8:43 AM | |
Posts: 8946 Rating: (999) |
MB 0 is used by default as flashing - bits. So it is better to use an other MB, i.e. M 2.0 and M 2.1, as constant signals. |
4/28/2014 8:55 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (23) |
Correct.. By default MB 0 used for clock memory if its enabled. |
Follow us on