4/28/2014 9:48 PM | |
Posts: 5225 Rating: (1185) |
Please supply a screen capture of your error.. or send us a program with your hardware configuration (assuming it is an hardware error) Thank you. w |
5/1/2014 10:10 AM | |
Posts: 5225 Rating: (1185) |
Hi there. I could not reproduce your problem. Are you using a PLC with hardware version 3? That is the one with the "31" in the part number. If not.. update your software. The attached program is what I think you are looking to create. I used TIA Portal V11 SP2 Update 5. If you give us the program you have tried, our forum friends will be able to do more. Please let us know your thoughts on the matter. Greetings. w AttachmentAssign x4 motion axis.zip (378 Downloads) |
2/4/2016 10:02 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by msige70 is split to a separate thread with the subject S7-1200 1215c problem in axis. Best regards |
Follow us on