9/8/2014 10:34 PM | |
Posts: 50 Rating: (0) |
Dear Friends, I bought New Simotion 6AU1445-0AA00-0AA0. Which i have replaced with Working 6AU1445 but its not working. Please see what steps i did. And guide me how can i fix this Issue. Please See PDF. I have adjust the Figures. 6AU1445-0AA00-0AA0 Please see the Figure3.Machine-6AU1445-ReadyThe Unit is working on machine perfectly. I get the working CF card ( Parameter and Program in CF Card ). And Insert in the New unit. And installed at the unit same location where theFigure 3Unit is installed. But the Status of 6AU1445-0AA00-0AA0 changes as Please see in Figure7.New-Machine-Operating-Status. 6AU1445-0AA00-0AA0 OK Status ( Machine Running ) Faulty Staus ( Machine Not Ready ) Ready ----- ON Ready ------ Blinking Run -------- ON Run --------- ON Stop ------- OFF Stop --------- ON SU/PF ---- OFF SU/PF ------ ON SF --------- ON SF ---------- ON DP1 ------- ON DP1 -------- ON DP2 ------- ON DP2 -------- ON OPT ------ OFF OPT -------- OFF If the parameters are not correct. Then why the Same CF card works in OLDER 6AU1445 which is currently working on machine. Note : One point which i have Noted. Older 6AU1445-0AA00-0AA0 hasVersion Eand New 6AU1445-0AA00-0AA0 has Version B. Please See the Figure1. Machine-6AU1445( Version E ) and Figure6.New-6AU1445( Version B ). Please compare both pictures and tell will it effect ? Has Both versions have the Same Configuration Files ? Please Guide how can i fix this issue. Waiting for your Support and Help THanks Regards, Umair Rasool
Attachment6AU1445-0AA00-0AA0 Pictures.pdf (190 Downloads) |
9/9/2014 4:54 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, the "green" cover on the D445, remove it, then you see the bcd display. Regards Christoph |
Follow us on