Industry Online Support
Technical Forum
9/12/2014 2:50 PM | |
Joined: 6/20/2011 Last visit: 5/21/2024 Posts: 74 Rating: (7) |
can i use this bit as an fisrtscan bit ? is this only 1 during the first cycle ? |
9/12/2014 3:38 PM | |
Joined: 6/20/2011 Last visit: 5/21/2024 Posts: 74 Rating: (7) |
See the Picture 2 bits are programmed as inputs on OB1 |
9/12/2014 3:53 PM | |
Posts: 88 Rating: (12) |
Yes "Initial_Call" should be the first scan bit. |
9/12/2014 4:16 PM | |
Joined: 6/20/2011 Last visit: 5/21/2024 Posts: 74 Rating: (7) |
Oke thanks..... |
Follow us on