9/24/2014 8:50 AM | |
Joined: 10/7/2005 Last visit: 5/6/2024 Posts: 3004 Rating: (1046)
|
Hello Marco_G
well, sort of, but it's more a case of you not taking AR2 into account which contains the Multi Instance offset when an FB is called. Have a look access to one multi-instance on how to do this and note that the command "UD DW#16#00FF_FFFF" is German menmonic and would be "AD DW#16#00FF_FFFF" in english mnemonic. I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
9/24/2014 9:26 AM | |
Posts: 8946 Rating: (999) |
That is exactly the point! Never forget AR2 if using a FB. Also if it is not called inside multiinstance, because you never know if it will be used as multiinstance one day... |
This contribution was helpful to1 thankful Users |
Follow us on