10/14/2014 12:10 AM | |
Posts: 2 Rating: (0) |
Hi, I would like to know if it's possible to connect a S7-1500 CPUwith a TP177B. I tried a procedure thatworked with the S7-1200 series. It worked fine, but when I tried it with the S7-1500 it didn't worked out at all. The procedure is the following: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=38112005&caller=view. (How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2?) Thanks in advance. |
2/15/2017 5:14 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by Space24 is split to a separate thread with the subject Connection between S7-1500 and TP177B. Best regards |
Follow us on