Industry Online Support
Technical Forum
10/30/2014 8:38 AM | |
Posts: 6 Rating: (0) |
Hi,I want to add a CPU that is not present in the library of TIA portal . Does someone can helpme ? |
10/30/2014 8:44 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello, That can only be done by using Hardware Support Package: Support Packages for the hardware catalog in the TIA Portal But perhaps you want a CPU, that is not supported by the version of TIA Portal you have. Please tell us the version of TIA Portal and the CPU you want to use? Best regards, Wizard |
10/30/2014 9:01 AM | |
Posts: 6 Rating: (0) |
I want to use CPU 315 - 2DP (6ES7315 2AF03-0AB0) with Panel OP270 CSTN 10" (6AV6542-0CC10-0AX0) in Tia portal V12, but i can't find this. |
10/30/2014 9:07 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello, Here is a link with more information: Which devices and modules are supported by STEP 7 Professional and WinCC Professional in the TIA Portal? I'm afraid your hardware is too old. You should use Step 7 Classic and WinCC flexible. Best regards, Wizard |
10/30/2014 9:09 AM | |
Posts: 6 Rating: (0) |
thank you even |
This contribution was helpful to1 thankful Users |
Follow us on