11/13/2014 12:31 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145) |
Hello Maxime Visconte, the function "MSRTCreateMsgInstanceWithComment" is a so called ODK-function,
that means a function, which is more "internal" in WinCC, as the internal or Standardfunctions, you can see in the C-Editor of WinCC. Maybe the following FAQ can you help http://support.automation.siemens.com/WW/view/en/24325381 There is an example (24325381_ISALG_OperationLog.fct) where the function "MSRTCreateMsgInstanceWithComment" is used. For more information about ODK see: http://w3.siemens.com/mcms/human-machine-interface/en/visualization-software/scada/wincc-options/wincc-odk/Pages/Default.aspx Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/11/2014 2:30 PM | |
Posts: 72 Rating: (2) |
IT WORKS!!!!! Thank you so much! This was one hell of a first post. Thanks again.
|
2/13/2017 1:09 PM | |
Posts: 9 Rating: (0) |
Thank you! Same problem, same solution solved it |
5/16/2017 10:01 AM | |
Joined: 8/4/2011 Last visit: 3/11/2024 Posts: 9 Rating: (0) |
We have the same problem here, and it works too! Thanks alot! Best Regards from Germany |
Follow us on