11/25/2014 3:13 PM | |
Joined: 7/26/2010 Last visit: 10/2/2023 Posts: 1 Rating: (0) |
Hi Dear I Need Windows CE ISO Image Download Link! for Mp377 12" Touch panel. Regards. ---------------------------- New subject after splitting from MP377 12". |
Last edited by: Hamid1977 at: 11/26/2014 7:23 AMLast edited by: Min_Moderator at: 11/25/2014 4:59 PMSplitted |
|
11/27/2014 10:54 AM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, Please tell us what exactly the problem you have. I do not think that Siemens will allow to share download link for Panels Windows CE.
|
Ayman Elotaify |
|
11/27/2014 3:04 PM | |
Posts: 1058 Rating: (93) |
Hello Hamid1977, a download link for Windows CE is not available for sure, as it would make problems with licensing.I assume you would want to do a factory reset or update. How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels? What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? regards |
This contribution was helpful to1 thankful Users |
12/3/2020 9:22 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by tecoch is split to a separate thread with the subject Image files for mp 377. Best regards |
12/7/2020 8:25 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
New question published by tecoch is split to a separate thread with the subject panel mp377 - need win ce 5 for reboot the hmi . Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on