12/12/2014 6:22 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
The LOGO! delivered with the password "LOGO". |
This contribution was helpful to1 thankful Users |
12/12/2014 6:24 PM | |
Posts: 7 Rating: (1) |
What I mean is that the network I try to connect the Logo to requiers a password to allow traffic.. |
12/13/2014 11:30 AM | |
Posts: 5225 Rating: (1185) |
|
12/13/2014 2:09 PM | |
Posts: 7 Rating: (1) |
Before my ip changes, does this link work for you guys? Thanks
|
Last edited by: Burner_Sweden at: 12/13/2014 2:09 PM |
|
3/30/2018 10:36 AM | |
Joined: 8/18/2011 Last visit: 9/9/2022 Posts: 14 Rating: (0) |
HI, I'm also trying to publish my logo webserver to internet but not able to do. why you are using this IP http://83.209.149.89:8080/?, instead of 192.168.1.200 which is your logo IP. |
3/30/2018 1:47 PM | |
Joined: 8/18/2011 Last visit: 9/9/2022 Posts: 14 Rating: (0) |
Hi This is my public IP 116.87.118.176 then should I proceed? Thanks a lot. Regards, Ryan |
3/30/2018 3:01 PM | ||||
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following FAQ: How do you enable and call the web server on LOGO! 8? Port forwarding in the router setting"Remote side":
192.168.1.200 "LOGO IP Address" Office PC"Local side": https://public IP Address:8080 https://116.87.118.176:8080 |
|||
Eng.Mohamed Ibrahim |
||||
Follow us on