12/14/2014 11:41 AM | |
Joined: 3/17/2013 Last visit: 12/25/2023 Posts: 480 Rating: (43) |
Hi These are various methods to stop the drive OFF1: OFF-1 means Normal Stop. Motor will stop in predefined time setin Parameter i.e. Ramp Down time/Deceleration time OFF2: OFF-2 means Coast to Stop. Means drive will inhibit pulses and Motor will stop by it self with its own Inertia OFF3: OFF-3 normally used with Emergency Stop or Quick Stop It is also available here /tf/WW/en/Posts/44413. Regards, Vijay |
12/17/2014 6:31 AM | |
Joined: 7/16/2012 Last visit: 4/28/2024 Posts: 37 Rating: (0) |
What does meaning of OC ? |
12/19/2014 1:37 PM | |
Joined: 3/17/2013 Last visit: 12/25/2023 Posts: 480 Rating: (43) |
Operating condition |
10/19/2016 9:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by arifinsabuz is split to a separate thread with the subject Control Word for S120 Drive at PZD 4/4. Best regards |
Follow us on