1/11/2021 5:46 PM | |
Posts: 9 Rating: (0) |
Hi Everyone, Can S7-1200 be configured as a Profinet slave? Thanks |
1/11/2021 6:12 PM | |
Joined: 9/27/2006 Last visit: 3/28/2024 Posts: 12249 Rating: (2660) |
Hello Kurt; You will have to get used to the specific language used by Profinet networks: an IO controller (~ master) communicates with one or more IO devices (~ slaves). And yes, the S7-1200 PLCs can act as IO controller to 8 Io devices. It can also act as IO device to an IO controller. When the IO controller is a S7 PLC, then the S7-1200 is called an i-device: https://support.industry.siemens.com/cs/ww/en/view/109478798 Hope this helps, |
Last edited by: dchartier at: 01/11/2021 18:13:52 |
|
This contribution was helpful to3 thankful Users |
1/13/2021 12:59 AM | |
Posts: 9 Rating: (0) |
Thanks, Daniel [snip] AttachmentMELSEC iQ-R PROFINET IO Controller Module User's Manual (Startup).pdf (460 Downloads) |
Last edited by: Jen_Moderator at: 01/14/2021 06:05:04New subject after splitting Last edited by: Jen_Moderator at: 01/14/2021 06:09:20Division of questions into separate topics. |
|
Follow us on