1/22/2015 7:23 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, Have a look here: Which version of STEP 7 Micro/WIN or S7-200 PC Access is compatible with which version of MS Windows and read the FAQ about your PC adapter, I think you have a problem there: Installation of the PC Adapter USB/USB Prommer Driver with STEP7 V5.5 Regards, Marcjan |
Problem solved? |
|
1/23/2015 7:53 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, Microwin works as far as i knowwith all windows 7 versions, The problem you have is in my opinion related to your PC/PG adapter and it's drivers. Can you show us a printscreen with all interfaces installed? Please note you have a PC adapter not a PC/ PPI cable. Is Microwin the only simatic program installed or do you have also Step 7 V5.x ? Regards, Marcjan Attachmentpc adapter.pdf (1626 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
10/19/2015 1:25 PM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3015) |
Hello, in the first listbox (S7Online...) is here a entry for MicroWin? Regards Chistoph |
10/2/2020 11:57 AM | |
Posts: 1 Rating: (0) |
how to do this? |
10/2/2020 1:54 PM | |
Joined: 9/21/2012 Last visit: 9/26/2024 Posts: 4167 Rating: (464) |
How to do what? |
This contribution was helpful to1 thankful Users |
Follow us on