11/22/2018 5:54 AM | |
Posts: 1 Rating: (0) |
Hi we use the S7 -1200 CPU 1214C DC/DC/DC PLC. attache hardware 16x16 DIDQ card , 13 bit analog input card. This PLC In between operation it is going into stop mode. DIAG LED blinking on DIDQ card and analog Input card. If i connect the PLC to TIA portal software Found the communication error. If Ping the PLC IP 192.168.0.1 through command promt it was not rechable the device. Please help us how we restore the PLC run mode. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/22/2018 9:02:49 AMNew subject after splitting |
|
11/23/2018 10:19 AM | |
Joined: 12/13/2011 Last visit: 2/13/2024 Posts: 145 Rating: (6) |
hello has tried to put the card in the hardware and make a download only hardware compatible devices |
12/15/2018 7:05 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi Sandy7, Check your configuration carefully. If you downloaded hw config. and your program you have to remember last window ask, do you want put your PLC back to RUN mode! Online mode you can also start your plc. If you can´t go online. Check your PC ip and like answer before, online mode you can see connections from project tree. Send more information if problem going on... regards Heksu reset ipto |
"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
Follow us on