2/7/2015 4:38 PM | |
Joined: 12/30/2014 Last visit: 1/19/2022 Posts: 10 Rating:
|
Hello Marcjan, Here is another one ... :-) : I have bought the Logo 0BA8 PLC and the Logo TDE ... and the LSC interface so I can continue the rest of the program. Finished 90% of it BUT when I try to write it to the PLC the LSC says : The diagram exceeds BM memory limit. Only block location is saved. ... I press OK and the whole program is written onto the Logo PLC ... or is it ? ... because some procedures in the program do not work ... :-) ! I went ahead and verified (pressed F2) my PLC needs ... and the 0BA8 was suggested ... and a list with program informations was written into the INFO Window, as follws: *** Determine LOGO! Resources used: Function Blocks 205/400 REM 72/250 Digital Inputs 6/24 Digital Outputs 3/20 Flag 36/64 Analog Inputs 2/8 Text Box 43/50 Text contents 44/50 Analog outputs 0/8 Program memory 2944/8500 Block names 0/100 Analog flags 0/64 Cursor keys 3/4 Shift register 0/4 Shift register bits 0/32 Open connectors 23/64 LOGO! TD Function keys 4/4 Network inputs 0/64 Network analog inputs 0/32 UDF types 0/16 UDF instances 0/64 Data Log 0/1 Network outputs 0/64 Network analog outputs 0/16 Analog Filters 0/8 Layout memory 49125/30000 Maximum nesting depth: M50-B180-B183-B196-B201-B232-B228-B134-B164-B063-M30 The following LOGO! can be used: 0BA8.Standard What does that mean ?! :-)
------------- |
Last edited by: Min_Moderator at: 2/9/2015 9:18:07 AMNew subject after splitting Last edited by: Min_Moderator at: 2/9/2015 9:20:31 AM |
|
Follow us on