2/18/2015 12:56 PM | |
Posts: 10 Rating: (0) |
Hi, LOGO!Soft Comfort v.7.1.5 support LOGO!TD or this problem in real button: INPUT: F1, F2, F3, F4 (ŠTART) - no problem , C1, C2, C3, C4 (see attachment) - simulacion in LOGO!Soft is OK, real malfunctioning as inputs !? OTHER: X0:PE - it is necessary to connect the ground PE to minus ( 0V ) - LOGO!Power ? PS: Blinker schematic, ŠTART (F1-F4), STOP & CENTRAL STOP is functioning ;-) LOAD / UPLOAD different scheme: (Ctrl+D) PC->LOGO! vs (Ctrl+U) LOGO!->PC - raggedness, chaos, more flag added |
3/10/2015 10:10 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
1/8/2016 9:15 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
New question published by AutoGen_914775 is split to a separate thread with the subject LOGO TD STARTUP MENSSAGE . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on