8/14/2015 10:30 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by Techspray is split to a separate thread with the subject S7-1200 stays in stop mode. Best regards |
3/3/2016 6:25 AM | |
Posts: 3 Rating:
|
HI I have the same problemm like RUBU.The plc goes in the STOP mode aftere a time of running.I proceeded the WARM RESTART procedure but after a time the same things it's hapening.I've attached the fault list wich i've downloaded from the PLC. Can someoane help me. Thank you! AttachmentDiagnostics.txt (630 Downloads) |
3/3/2016 8:53 PM | |
Posts: 3 Rating:
|
Thanks for your suggestions Best regards |
This contribution was helpful to
1 thankful Users |
4/26/2016 7:53 PM | |
Posts: 1 Rating:
|
Hello, I have a similar problem but only one of my PLC's has gone to STOP mode and even when I connect with the TIA PORTAL and try to run it from the program, it wouldn't change or even when I upload a new program it won't change the STOP mode. I'm attaching the diagnostics so maybe someone can help me. AttachmentDiagnostics.txt (465 Downloads) |
Follow us on