3/16/2015 12:50 PM | |
Posts: 567 Rating:
|
Hi,
I think you also need the SimaticNet HardNet - IE S7 license. You can find more information in the PCS 7 catalog on page 5/13. You can download the catalog under the following link: http://w3app.siemens.com/mcms/infocenter/content/en/Pages/order_form.aspx
|
3/16/2015 9:05 PM | |
Posts: 2 Rating:
|
Thank you for the response. Unfortunately PCS7 V8 catalog shows V8.1 licenses (which we bought) while the PCS7 V8 SP1 disk installs SimaticNet v8.2 making the purchased licenses useless. We then bought new licenses based on what the V8.1 catalog says on page 5/18 (see below) I'm getting a little frustrated spending time and money on this one. If I have to buy it then I will but if it something else simple I need to do without spending all that money I will. My client has about had it with PCS7 licensing issues. Catalog 5/18 Activation license if no redundant AS are used Activation licenses when using redundant AS
|
9/30/2015 3:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating:
|
New question published by U_cc88a8a2-3886-4746-a888-fe83b9af5c30 is split to a separate thread with the subject What is the correct type and quantity of HARDNET licences. Best regards |
Follow us on