3/16/2015 8:38 PM | |
Joined: 10/24/2006 Last visit: 11/23/2022 Posts: 15 Rating: (1) |
I think I have quit the same problem, I'm trying to make an off delay depending on how long the input is on. But to prevent the couter goes up to 999999 I want to put in a max for example on 600 s. In the example m3 is a pulse every second. I3 is the input for the offdelay. So when 10 seconds on, the offdelay should be 10 seconds after I3 is off. As max I'm searching for a function where I can compare the value from the counter with the max value for example 600 for 10 minutes. I got also a problem that I can not choose a reference parameter for an offdelay. Is there a way to enable this or depents this on the kind of logo?
---------------------------------------------------------------------------------------------------- |
Last edited by: Schampbakken at: 3/16/2015 9:21:53 PMLast edited by: Min_Moderator at: 3/17/2015 9:33:32 AMNew subject after splitting |
|
3/16/2015 9:33 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32817 Rating: (4061) |
For the new way of reference look here: https://support.industry.siemens.com/cs/document/109471094?pnid=13617&lc=en-DE |
Follow us on