3/22/2015 10:47 AM | |
Joined: 1/15/2015 Last visit: 3/22/2022 Posts: 66 Rating:
|
Dear experts ; This is iz Aljabre from Jordan welcome to all May i ask: In which situations the CPU will ask for stop to download your modified code in S7 ? thank you in advance
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/24/2015 2:19:28 PMNew subject after splitting |
|
3/22/2015 11:31 AM | |
Joined: 1/28/2009 Last visit: 6/26/2024 Posts: 6841 Rating:
|
If we are talking about STEP 7 basic package for SIMATIC S7-300/400 CPUs , normally extra checks on your codes are not mandatory and you can download your modified codes to CPU with your own responsibility.CPU never asks your permission to enter in STOP mode because of programming error .There are some routine check before you implement your change and finalize them.Also some minor warning you receive while editing your program (attached file).To avoid entering CPU to STOP mode the following OBs are suggested to be downloaded to CPU and react to cause of error and possibly shutdown part of plant . Which organization blocks do you need for error handling in STEP 7 V5.5? |
This contribution was helpful to
1 thankful Users |
Follow us on