3/23/2015 8:52 AM | |
Posts: 19 Rating: (0) |
Hi, I am also using the VMxnet3 Ethernet Adapter driver and TIA V13 SP1, Server 2012 R2. I can't go Online and I could it before. I have tried to install everything on a new Server but same result. I can ping the PLC but i can't go online. I am using a router to connect to our production network. Is there anyone who can have an idea of what is causing this problem. I have TIA on my own computer and there I have no problem to connect to the PLC. But there I can use the Ethernet interface instead but not on the server there I can only choose PN/IE? Br
|
Last edited by: Min_Moderator at: 3/24/2015 4:30:16 PMNew subject after splitting |
|
7/9/2015 1:26 PM | |
Joined: 5/9/2011 Last visit: 9/24/2024 Posts: 71 Rating: (5) |
Sepes, did you select the "use IP router" in the dialog box of the communication properties? |
Follow us on