(0)| 3/31/2015 2:22 PM | |
|
Joined: 12/26/2010 Last visit: 4/10/2025 Posts: 27 Rating:
|
Hi, I have a similar situation: I need Rx3i (GE PLC) to be PN master and S7-315 to be slave. I configured the s7-315 as IO device and exported the gsd file. The GE programming software (PME) got the file but was faulted when downloading to PLC. GE support answer me that @ the gsdml file there are 2 parameters called "FixedInSubslots" and their values are 1000 &1001 but GE PLC knows to deal just with slaves range 0-255. gsdml file is attached. I changed the values to 100 & 101 and downloaded to GE PLC and it's running but no comm. with s7-315. The s7-315 itself is running but with fault led red. I assume I need to change the values somewhere @ the s7-315 but where and how ? ---------------------------------------------------------------------------------------------------- AttachmentGSDML-V2.25-#Siemens-PreConf_S7300prof1-20150326-134152.zip (193 Downloads) |
Last edited by: Min_Moderator at: 3/31/2015 4:54:56 PMNew subject after splittting |
|
Follow us on