4/7/2015 6:28 PM | |
Posts: 30 Rating: (0) |
Hello, I try to import the XDB file using station configuration editor, firstly i get this error "configured component was remplaced by an existing component!", i skip this error, After the loading of the component, the IE General showing stop, i try to run it by Right click on it / Run, the IE General start for a few seconds then stop again. I read this topics: Configuration Station IE General is showing me STOP mode IE General STOP in Station Configurator But the problem was not resolved yet, please can any one help to resolve this problem. Thanks in advance |
4/8/2015 4:11 PM | |
Posts: 30 Rating: (0) |
Hi , thank you so much for your response, please find in attachment two images that show the IP adresse for the IE General and the Local Area Network. The two adresses are the same but i still have this problem, any suggestions please ; Attachmentimg.rar (520 Downloads) |
4/9/2015 6:39 PM | |
Posts: 30 Rating: (0) |
Hi can any one help please? ragards |
Follow us on