4/10/2015 12:45 AM | |
Joined: 11/10/2010 Last visit: 12/3/2023 Posts: 24 Rating: (0) |
Hello all I need help to communicate with WinCC RT.The PLC s7 200 works with Syswin without any problem but RT doesnt.The adress of Panel and the PG are the same,the configuration of the panel under wincc is good but the link doesn't work!I utilize MPI/USB adapter which is ok. The panel is Touch 10",the PLC s7 200 cpu 224 Thank you for help
|
Last edited by: Min_Moderator at: 4/10/2015 1:01:12 PMNew subject after splitting |
|
Follow us on