4/15/2015 8:56 AM | |
Posts: 3 Rating: (0) |
Hi, I also have same problem so I need same help |
4/15/2015 8:58 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3015)
|
then provide the information ! screenshot of error message? |
4/15/2015 9:14 AM | |
Posts: 3 Rating: (0) |
Hi, I attached 2 pictures, 1 my operating system 2 the error massage I receive thanks for your help AttachmentError.rar (302 Downloads) |
4/15/2015 9:37 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3015)
|
Hello, you have a other problem like the first poster! You get the message at the begin of the installation not after the setup if you start the SCOUT! To solve your problem you should follow the steps in the FAQ SIMOTION, SCOUT: "SCOUT cannot be installed on WINDOWS VISTA" under Windows 7Regards |
This contribution was helpful to1 thankful Users |
4/15/2015 9:48 AM | |
Posts: 3 Rating: (0) |
Hi, thanks for your kind reply, timing different but result same :) |
This contribution was helpful to1 thankful Users |
4/15/2015 11:42 AM | |
Posts: 4 Rating: (0) |
Thank you very much! I have already done! :D |
Follow us on