4/15/2015 10:31 AM | |
Joined: 3/18/2010 Last visit: 3/6/2024 Posts: 8 Rating: (0) |
Hello, I have the following configuration: 1x IM 151-8 CPU PN/DP - 6ES7151-8AB01-0AB0 1x PM-E 24V DC - 6ES7138-4CA01-0AA0 12x 8DI, 24V DC, standard - 6ES7131-4BF00-0AA0 4x 8DO, 24V DC/0.5A, standard - 6ES7132-4BF00-0AA0 4x 4AI, I, standard - 6ES7134-4GD00-0AB0 4x 2/4AI, RTD, standard - 6ES7134-4JB51-0AB0 1x 1 Count 24V/100kHz - 6ES7138-4DA04-0AB0 My question is: can I identify which of DI/DO is faulty if these cards don't have diagnostic function? I am using Tia Portal V13.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/15/2015 2:59:21 PMNew subject after splitting |
|
4/16/2015 3:19 PM | |
Posts: 366 Rating: (30) |
yes then I would prefer some kind of software surveillance like mentioned above if possible! What are you switching with the outputs? regards |
4/20/2015 12:00 PM | |
Posts: 366 Rating: (30) |
You can realize this surveillance with a normal 8DI input card. You don't need HF.. nice regards |
Follow us on