4/28/2015 11:00 AM | |
Posts: 41 Rating: (0) |
Hello, experts! I have problems when trying to simulate PID controller. Program is created on TIA V13, CPU is 1212 V4.1 DC/DC/DC , PID_compact is V2.2. 1st problem: When I start simulation of the program, the pid goes in inactive mode, seen in the comissionning window. In the data block STATE=0, error double word=0, MODE=3 (Auto). 2nd problem : When I click on the icon for the comissionning or the configuration window TIA portal crashes. 7 times for 2 hours today.
---------------------------------------------------------------------------------------------------- Attachmentproblem.rar (152 Downloads) |
Last edited by: iv73nikolov at: 4/28/2015 11:03:20 AMLast edited by: iv73nikolov at: 4/28/2015 11:05:46 AMLast edited by: Min_Moderator at: 4/28/2015 11:44:25 AMNew subject after splitting |
|
Follow us on