4/29/2015 2:24 PM | |
Posts: 5 Rating: (0) |
Hello , I am using PSC7 ver 8.0 with WinCC ver 7.2 Update 9 and PLCSIM ver 5.4+SP5+Upd1.Its running on windows 7 As i am trying to simulate my program through simulation i am getting error that SDB7 can not be loaded,at this time PG/PC interface is on PLCSIM/Local.When i have set PG/PC interface on PLCSim/TCP1 then i am getting error that SDB2000 can not be deleted. beacuse of this error i am unable to download my program and run WinCC in simulation. I have tried with different set of hw combination but i am still getting same error. I am providing current set of hw combination what i am using. PS407 10A CPu 416-2DP CP443-1 6GK& 443-1EX20-0EX/v2.0 WinCC application with IE_CP/V6.2.1 Please suggest me what should i made changes so i can simulate the program. Please help...pleaseee
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/29/2015 4:29:01 PMNew subject after splitting |
|
4/30/2015 9:44 AM | |
Posts: 567 Rating: (106) |
Hello, did you try to use PLCSIM.ISO, too?
|
This contribution was helpful to1 thankful Users |
4/30/2015 11:59 AM | |
Posts: 5 Rating: (0) |
Nope ..i havent tried...i will try and revert |
4/30/2015 12:13 PM | |
Posts: 5 Rating: (0) |
Hello I trie with ISO also but i am getting same error ..SDB 7 can not be loded and the function is not permitted in the current protection lelvel. |
Follow us on