5/29/2015 8:34 AM | |
Posts: 6 Rating: (0) |
is it possible to communicat s7 300(in TIA V11 PORTAL)...and SIMATIC WINCC FLEXIBLE SP2 2008... please reply me as fast. as posssible.... HMI model TP177A.... and IN HMI.... i am NOT getting to add option to ADD TP177A IN TIA
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/29/2015 9:23:21 AMNew subject after splitting |
|
5/29/2015 9:34 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, I think is almost the same with S7 300: how do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? |
Follow us on