(1)| 6/15/2015 9:20 AM | |
|
Joined: 5/20/2015 Last visit: 1/15/2026 Posts: 222 Rating:
|
hey dear, your guidance is such a useful, Presently i am working with IWLAN ACCESS POINT (SCALANCE W774-1 RJ45) and IWLAN CLIENT (SCALANCE W722-1 RJ45) on TIA V13. CPU is S7-1214, please provide me a SAMPLE PROGRAM about integration and settings of Above hardware, for TIA side Only ASAP. Note: communication is done b/w Access Point And client point, only TIA side work is Remaining. thank you.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/15/2015 4:26:13 PMNew subject after splitting Let's do it... |
|
| 6/15/2015 9:42 AM | |
|
Posts: 1058 Rating:
|
Hello gabbar, here you are: IWLAN: Setup of a Wireless LAN in the Industrial Environment regards |
Follow us on