6/17/2015 11:31 AM | |||||||||
Joined: 5/12/2006 Last visit: 5/13/2024 Posts: 22244 Rating: (2983) |
Hi, https://support.industry.siemens.com/cs/ww/en/view/50105638
In the case of a spare part replacement:
When you employ a compatible follow-up type, you can always work with the order no. of the predecessor type in the STEP 7 project. Configuration with older software versions:
It is not necessary to upgrade the STEP 7 software in this case either. Regards Christoph |
||||||||
This contribution was helpful to2 thankful Users |
6/17/2015 12:50 PM | |||||||||||||||
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
this is not necessary. As you can see in following FAQ, both CPU313 can work with every Simatic MMC with max. 8MB. Which memory cards can you use with an S7-300 CPU?you can also see in the delivery release of the new CPU, that it is compatible with all existing Simatic MMC:SIMATIC Micro Memory Card (required for CPU operation)
hope this helps,regards, |
||||||||||||||
FCK WAR! |
|||||||||||||||
This contribution was helpful to1 thankful Users |
6/18/2015 5:19 AM | |
Posts: 153 Rating: (9) |
thanks you |
Follow us on