6/22/2015 9:31 PM | |
Posts: 2 Rating: (0) |
Hello! I have a problem with PLCSIM V13 for S7-1200. When I try to simulate a simple function (picture 1). My set/reset block don't work correctly . When there is a signal on B1 and B2 set/reset block sends a signal through Q to turn on M1 (Picture 2). But as soon as B2 or B1 signal is lost the block loses as signal on Q (picture 3). Set/reset block should save the signal wance is turned on, until there comes a signal on B3 and resets a block. Any idea why this is not working correctly? Thanks!
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/23/2015 1:45:25 PMNew subject after splitting |
|
6/24/2015 1:51 AM | |
Posts: 2 Rating: (0) |
Thanks! It works! |
This contribution was helpful to1 thankful Users |
Follow us on