7/6/2015 8:57 PM | |
Posts: 2 Rating:
|
I can not seem to figure out the correct settings and or way to load a G-Code program into my Hyundai Lathe with the Siemens 840c control. I am able to send a known and working program out of the control to my xlTransfer box with usb then open it on my PC, but I can not figure out how to get it back in the control. The Siemens 840c control should accept standard G-Code from my understanding but when I try sending the program over I keep getting alarm code 110032 " Error in Archive File" then the transfer stops. Can any one on here help or have advice on where to find a "usable" manual for this issue? I called the people who sold me the box and they say it is Siemens settings. They say I need to know exactly what the control is looking for such as start of program % end of program % EOB Character? I called Siemens and they say they will look into it... I understand that the 840c should accept standard program format such as
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/7/2015 11:12:02 AMNew subject after splitting |
|
7/13/2015 5:47 PM | |
Posts: 2 Rating:
|
Thank you |
Follow us on