7/10/2015 11:36 AM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating: (4) |
Hello All, I am newbie in PCS7. I have programmed CFC by using PID blocks and Monitoring blocks. After that i have compiled the same "Chart as block type". Now when i am using this block in another CFC, no block icon is created for the blocks which were used to program the block i.e. PID and Monitoring block. Can you please suggest me the procedure to create the block icons in this case. Thanks in advance! Best regards, Naresh Saini
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/10/2015 2:57:34 PMNew subject after splitting |
|
7/16/2015 1:18 PM | |
Posts: 567 Rating: (106) |
Hi nrk, I think it is not possible to create block symbols for blocks which are part of a chart that was compiled as block typ. This statement you can find in the CFC manual: I think using block symbols is another example for externally access. You can find more information under the following link: |
Follow us on