7/11/2015 6:53 AM | |
Posts: 1 Rating: (0) |
Hi.. I am working on a project where we need to put the PLC in a control room which is away from the field but the manual push button station will remain in the field. There are around 50 DI and 70 DO. All the DI and DO to be kept in the field panel but their contact need to fed to PLC which is in control room long away from the field. To make cabling for these number of DI and DO, we will require huge amount of cabling. My query is: Is there any way to establish any communication system which will take less cabling but will work efficiently? Is there any way to make serial synchronous/asynchronous mode of communication between two panels? Thanks
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/13/2015 1:14:55 PMNew subject after splitting |
|
Follow us on