7/30/2015 11:38 AM | |
Joined: 6/2/2015 Last visit: 11/21/2023 Posts: 1 Rating: (0) |
Hello,
I'am trying to create a popup wich must be activated by an alarm in a PLC (s7-400). I created a tag on a bit from the PLC. (The PLC is not in the tia portal project). For some reason i can't select the show pop up screen options under the events of this tag. When i use a button i can select the option show pop up screen but who wants a pop up if you first have to press a button.
Who nows the solution?
Thanks,
Jan van Bentum
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/30/2015 12:00:20 PMNew subject after splitting Last edited by: Min_Moderator at: 7/31/2015 9:28:37 AMChange Tip -> Topic |
|
9/1/2015 8:02 AM | |
Joined: 3/12/2015 Last visit: 2/20/2024 Posts: 2 Rating: (0) |
I'm trying to get the same function. If there is anybody with a good idea how to work this out I would be grateful! |
Follow us on