(0)| 8/3/2015 2:55 PM | |
|
Posts: 20 Rating:
|
Dear experts; I need some information about the simocode pro V digital inputs. I need to know wich voltaje levels accepts for "0" logic and "1" logic. I could not find the information that I need (current , voltaje). I require this is because someone in our department is getting a MCC from siemens with this simocode prov, but I believe that no one think about the distance for 24 DC (800 meter single, so 1.4 km total), The use will be for dry contacts and I need to know the information for calculations. Best regards hp ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 8/3/2015 3:38:34 PMNew subject after splitting |
|
Follow us on