8/5/2015 7:59 PM | |
Posts: 111 Rating: (1) |
I was going through the logic and find few bits whom doesn't have any addresses I am mentioning those bits at the bottom with a red mark if anyone can tell how to find the address of these bits or what these bits can be and they have no cross reference but when i try local application instead of cross reference then it helps in finding out something with the same name as these bits.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 8/6/2015 9:47:41 AMNew subject after splitting |
|
8/5/2015 9:16 PM | |
Posts: 111 Rating: (1) |
but the thing is I can reach the o/p but want to know exactly why addresses are not defined for these bits and How PLC is reading it. |
8/6/2015 9:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on