8/9/2015 12:57 PM | |
Posts: 2 Rating: (0) |
Hello there, I need a urgent help. i m very new to PLC :( Struggling to get the Device online . Could anyone please help to make hardware Setup and software configuration using CPU 315-2 DP and PA device. Harwares i have: - PS 307 5A ( Power supply) - Siemens DP/PA coupler - CPU 315-2 DP(Firmware V3.3) - Siemens PC USB adapter Softwares i Have: Step 7 V5.5+SP2+HP4 SIMATIC PDM V8.0+SP2 SIMATIC PC ADAPTER USB V1.2 So i m trying to communicate to a PA device using above Software and hardware. HARDWARE connections: i have powered up the DP /PA coupler and CPU using PS 307 CPU DP terminal to DP/PA coupler CPU MPI terminal to PC USB I can only see the CPU only in the accessible nodes, can t get the device online. please help me on this. let me what s wrong i m doing here. Thanks!!!!
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 8/10/2015 2:52:53 PMNew subject after splitting |
|
8/9/2015 5:02 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello jupiter; You will never see the instrument in Additional Nodes,, this is only for programmable units (CPUs). You should start with setting up the Profibus network, and integrate the gsd file for the instrument. What exactly do you plan to connect as a Profibus-PA slave? Do you have the gsd file for it? The DP/PA coupler, if used standalone (outside of a DP/PA link setup) will not be shown in the HWConfig editor for the Profibus network, it is transparent to the Profibus-DP configuration. But the speed pof the bus must then be reduced to the Profibus-PA speed, 45,45 kB. So start with that, and look up more information in the following FAQ:
How do you set up the DP/PA link and how do you configure the DP/PA link and DP/PA coupler? Show us what you have as a Profibus configuration, and we can help you further. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/9/2015 6:20:49 PMLast edited by: dchartier at: 8/9/2015 9:09:03 PMLast edited by: dchartier at: 8/9/2015 9:09:33 PM |
|
This contribution was helpful to1 thankful Users |
8/10/2015 10:31 AM | |
Posts: 2 Rating: (0) |
Hello Daniel, Thanks Much for so quick response. I m planning to use the Fisher controls DVC6200p Device as Profibus PA Slave. I have Integrated the GSD for the same too. I m attaching a Document and a video , it will show exactly what i m trying do. What mistake i m making Please Use the following link to download the Video
https://emerson.sendthisfile.com/gKDtKtPTTu7VmTi1EWG8pT5J
PLC & PDM Config problem.zip
OR click here to download your file(s)
PLC & PDM Config problem.zip https://emerson.sendthisfile.com/c.jsp?t=FoasePblWnajOgtMX82wIpOn&n=gKDtKtPTTu7VmTi1EWG8pT5J Thankyou So much again for helping me in this. AttachmentPLC PDM.docx (211 Downloads) |
Last edited by: jupiter09 at: 8/10/2015 11:04:29 AM |
|
Follow us on