8/10/2015 2:32 PM | |
Posts: 33 Rating: (2) |
Hello Robster, I am trying to configure my S110 drive via pulse interface and S1200 motion control TO. When I tried to do commissioning from my TIA portal, it is running, but my drive doesn't run at all. Probably I have missed some drive parameters. I do the drive commissioning by STARTER software and used the wizard to configure the data exchange for pulse/direction control. I can also see from the STARTER, drive enable input (I0.0) is giving from the PLC motion control TO. So can you tell me the required drive parameters to check? Thanks.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 8/10/2015 4:22:55 PMNew subject after splitting |
|
8/10/2015 4:25 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on