8/13/2015 10:22 PM | |
Posts: 5 Rating:
|
Hi master I have a problem with the S5 115U CPU 944B current cpu is often difficult to stop yourself and reset , all the red light is on , the error machined to demonstrate the value of full loadcell when actually empty . CPU has been tried in the locker but still a problem , but if the EPROM is removed and reset cpu can instantly RUN but the program does not run perfectly . whether its EPROM problematic ? how to fill the EPROM without PG ? I tried online but there is an error in the computer " PC timeout " or " AG interface in PG not ready " or " undefined character .. " , what's the solution ? please help the good master ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/14/2015 9:39:19 AMNew subject after splitting |
|
8/14/2015 9:59 AM | |
Posts: 8946 Rating:
|
Do you have Simatic - PG with Step5 Software? You use the correct AS511 cable? Do you have the original Step5 application? |
8/19/2015 6:55 PM | |
Posts: 8946 Rating:
|
Answer questions first. Otherwise it is hard to help you. |
Follow us on