8/19/2015 5:37 PM | |
Posts: 16 Rating: (0) |
Hi, I have 1510SP-1PN CPU, Comfort Panel TP900 and TIA V13SP1Upd3 My problem: I have data in PLC in arrays of Real, INT and BOOL. From HMI I can define indexed tag to read data from the REAL and INT arrays. But when I try to do the same for BOOL Arrays I get the message: "Invalid Data Type ...". With S7 1200 CPU is working without problems I see that the driver in HMI is for S7 1500 so I think that is not linked with the CPU type (I have doubts that it work for 1200 and for 1500 not but who knows..) Can somebody tell me if I can solve the problem or I have to change the CPU? :( Thanks in advance! Adrian ------------------------------------------------------------------------------------------ |
Last edited by: aditzu at: 8/19/2015 5:38:54 PMLast edited by: Min_Moderator at: 8/20/2015 10:24:02 AMNew subject after splitting |
|
Follow us on