9/4/2015 11:41 AM | |
Joined: 5/13/2015 Last visit: 5/21/2024 Posts: 11 Rating: (0) |
Dear Pee,
machine with 840d control and motor with brake is giving alarm during SI test. Y-axis brake failure alarm. we interchange the motor from other machine, now it is working correctly. in SI test what parameters are used to test the brake? it is a vertical axis if brake fails means the whole thing should be come down? i am facing the same problem in so many machines? we have sent the motor to siemens the result yet to come. can you guide me how to over come from this problem.. thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/4/2015 2:07:54 PMNew subject after splitting |
|
Follow us on