9/23/2015 12:08 PM | |
Joined: 3/29/2012 Last visit: 10/8/2023 Posts: 61 Rating: (0) |
I have similar problem too but in my own case the step 7 V5.5 is installed in a VMware with operating system of window xp. while my main computer operating system is window 7. I cannot established connection between my laptop and the PLC using the PC adapter. I checked the device manager in my main computer to see if the PC adapter is connected, I could find it but it show error Icons that show that the driver for the PC adapter is missing. I checked through the site if I can download the driver for window 7 but i cannot find any driver for window 7. can any one assist on how to go about it? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/23/2015 2:40:35 PMNew subject after splitting johnluck |
|
Follow us on