9/26/2015 7:31 PM | |
Posts: 14 Rating: (0) |
Hi , I am using S7 V5.5.4 with PDM V8.0.1 & have similar problem. I have a project with PA devices but while engineering seems EDD is not assigned for GSD in HW Config. Now i am in commissioning & if i double click on slave from HW Config nothing happens/no popup & If i right click on slave -> SIMATIC PDM tab is inactive. How can i assign EDD to the existing slaves? But if i add new slave it popsup device assignment list & works fine for the new devices. where can i download SP2 for PDM V8.0? can you send me some link for the same? Thanks in Advance !!! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/28/2015 4:49:02 PMNew subject after splitting |
|
7/28/2016 1:44 PM | |
Posts: 111 Rating: (15) |
If you have to upgrade your PDM to PDM v8.0 incl. SP2: See following link for more information SIMATIC PDM V8.0 incl. Service Pack 2 Released for Delivery |
Follow us on