10/18/2015 1:17 PM | |
Posts: 1 Rating: (0) |
Dear all... In sinamic G120 P have a profi bus connection with 317-2 dp PLC module . Some time the drive displays the fault code of (F1910) . I checked tha fault code with drive manual which shows that was profibus communication problem. What are the remedy for that problem.....?
Thanks & Regards K.Gowthaman ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/19/2015 11:04:08 AMNew subject after splitting |
|
10/20/2015 10:27 AM | |
Posts: 58 Rating: (1) |
Greetings, Check parameter p2040. increase the time, it may help. best regards. |
Follow us on