(0)| 11/1/2015 9:42 AM | |
|
Posts: 4 Rating:
|
Good Day All I have issues regarding S7-1200 (Cpu1215 ). Basically we are trying to print pass or fail label with date to intermec printer pc43t, using cm1241 module via rs 232. The problem is our send ptp block works fine but absolutely no response from printer. When connecting from comms module to laptop via serial comms test program we can see info transmitted.The printer however does not respond in any way. We have tried straight connection using pins 2, 3 and 5 as well as crossover ( 2-3 ) but still no joy. Can anyone please assist with sample program regarding commands to send to this particular model intermec printer?? Any help would be highly appreciated! Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/1/2015 11:14:52 PMNew subject after splitting |
|
| 11/11/2015 12:00 PM | |
|
Posts: 5521 Rating:
|
hi NAZEER, How are the parameter-settings of the module? Check if the settings of the printer and the module are matching. When the module is sending or receiving there is a normally a LED blinking(Rx/Tx). Have a look in the manual of the S7-1200 PLC´s. In chapter 12 you will find some Information of the CP´s. SIMATIC S7 S7-1200 Programmable controllerhope this helps, regards, |
Follow us on